As partner to leading telecom operators worldwide, Prysmian Group produces and manufactures a wide range of cable systems and connectivity products used in telecommunication networks. The product portfolio includes optical fibre, optical cables, connectivity components and accessories and copper cables.
Optical fibre
Prysmian Group is one of the leading manufacturers of the core component of every type of optical cable: optical fibre. The Group is in the unique position of being able to use all existing manufacturing processes within its plants: MCVD (Modified Chemical Vapour Deposition), OVD (Outside Vapour Deposition), VAD (Vapour Axial Deposition) and PCVD (Plasma-activated Chemical Vapour Deposition). The result is an optimised product range for different applications. With centres of excellence in Battipaglia (Italy), Eindhoven (the Netherlands) and Douvrin (France), and 5 production sites around the world, Prysmian Group offers a wide range of optical fibres, such as single-mode, multimode and specialty fibres, designed and manufactured to cater to the broadest possible spectrum of customer applications.
Optical cables
Optical fibres are employed in the production of standard optical cables or those specially designed for challenging or inaccessible environments. Optical cables, constructed using just a single fibre or up to as many as 1,728 fibres, can be pulled (or blown) into ducts, buried directly underground or suspended on overhead devices such as telegraph poles or electricity pylons. Cables are also installed in road and rail tunnels, gas and sewerage networks and inside various buildings where they must satisfy specific fire-resistant requirements. Prysmian Group operates in the telecommunications market with a wide range of cable solutions and systems that respond to the demand for wider bandwidth by major network operators and service providers. The product portfolio covers every area of the industry, including long-distance and urban systems, and solutions such as optical ground wire (OPGW), Rapier (easy break-out), Siroccoxs (fibres and cables for blown installation), Flextube® (extremely flexible easy-to-handle cables for indoor or outdoor installations), Airbag (dielectric direct buried cable) and many more.
Connectivity
Whether deployed in outdoor or indoor applications, Prysmian Group's OAsys connectivity solutions are designed for versatility, covering all cable management needs whatever the network type. These include aerial and underground installations, as well as cabling in central offices (or exchanges) or customer premises. Prysmian Group has been designing, developing and making cable and fibre management products for more than two decades and is at the forefront of designing next-generation products specifically for Fibre-To-The-Home (FTTH) networks.
FTTx
Increasing bandwidth requirements, by both business and residential customers, are having a profound effect upon the level of performance demanded of optical networks, which in turn demands high standards of fibre management. Optimal fibre management in every section of the network is increasingly a matter of priority in order to minimise power loss and overcome the problems caused by ever greater space limitations. The Group has developed the suite of xsNet products for "last mile" access networks, which is also very suited to optical fibre deployment in sparsely populated rural areas. Most of the cables used in FTTx/FTTH systems feature Prysmian's bend-insensitive BendBrightxs optical fibre, which has been specially developed for this application.
FTTA (Fibre-To-The-Antenna)
xsMobile, which offers Fibre-To-The-Antenna (FTTA) solutions, is an extensive passive portfolio which enables mobile operators to upgrade their networks quickly and easily. Incorporating Prysmian's experience in Fibre-to-the-Home (FTTH) and its unique fibre innovations, xsMobile provides different product solutions for three applications: antenna towers, roof-top antennas and Distributed Antenna Systems (DAS) for small cell deployment. The technology offers three access types for outdoor and indoor FTTA deployment, as well as backhaul solutions, incorporating the latest fibre technologies.
Copper cables
Prysmian Group also produces a wide range of copper cables for underground and overhead cabling solutions and for both residential and commercial buildings. The product portfolio comprises cables of different capacity, including broadband xDSL cables and those designed for high transmission, low interference and electromagnetic compatibility.
Multimedia Solutions
The Group also produces cable solutions serving communication needs in infrastructure, industry and transport, for a diverse range of applications: cables for television and film studios, cables for rail networks such as underground cables for long-distance telecommunications, light-signalling cables and cables for track switching devices, as well as cables for mobile telecommunications antennae and for data centres.